Bluetooth Workshop
This material is 2 of 6 in the Bluetooth 181 - Workshop (SSv4): Develop a Secure IoT Device on a BG22 Thunderboard Kit.
This Bluetooth workshop provides hands-on training and teaches users how to develop and deploy ultra-low-power, secure Bluetooth connectivity with the BG22 with Simplicity Studio v4.
This Bluetooth workshop provides hands-on training and teaches users how to develop and deploy ultra-low-power, secure Bluetooth connectivity with the BG22 with Simplicity Studio v4.
Overview
The hands-on lab for the first day helps get the user set up with the Simplicity Studio Version 4 tool suite. The user learns how to create a project, set GATT parameters and then flash/program the Thunderboard BG22.
Lab materials are available for users to follow along with the instructor in this video.
Language Choice:
Prerequisites:
Lab Guide: Out of the Box Thunderboard Example Project
Hardware Required:
Thunderboard Kit EFR32BG22
(SLTB010A)