Matter Developer Journey With Silicon Labs

Silicon Labs can accelerate the development of Matter devices, starting by outlining each step in the process and helping you along each stage of your project. Guiding you along the path of ecosystem partners. We’re happy to simplify your development journey and help you get your device to market faster and more efficiently.

We’ve outlined below three key stages of your journey, along with what’s required to successfully complete each stage.

Getting Started
Develop
Deploy Product
  1. 1. Learn and Explore
  2. 2. Choose Your Hardware Platform
  3. 3. Buy Your Dev Kit
  4. 4. Create User Accounts
  5. 5. Set Up Dev Environment
  1. 1. Develop Your Product
  2. 2. Test & Iterate
  3. 3. Certify Product
  1. 1. Manufacture Product
  2. 2. Operate Product

1. Introduction to Matter

Matter: A Unified Approach to IoT Device Development

Matter drives the convergence between the major IoT ecosystems to create one easy, reliable, and secure wireless protocol to connect all IoT devices and networks.
 

Additional Resources from Silicon Labs



The connectivity Standards Alliance is the standards defining organization for Matter. matter was created on the promise of reliable and secure connectivity.
 

Additional Resources from CSA

What is Alexa?

Alexa is Amazon’s cloud-based voice service available on hundreds of millions of devices from Amazon and third-party device manufacturers. With Alexa, you can build natural voice experiences that offer customers a more intuitive way to interact with the technology they use every day. We offer a collection of tools, APIs, reference solutions, and documentation to make it easier to build for Alexa.

What is Google Home?

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat. Duis aute irure dolor in reprehenderit in voluptate velit esse cillum dolore eu fugiat nulla pariatur. Excepteur sint occaecat cupidatat non proident, sunt in culpa qui officia deserunt mollit anim id est laborum.

Google Home Resources

What is SmartThings?

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat. Duis aute irure dolor in reprehenderit in voluptate velit esse cillum dolore eu fugiat nulla pariatur. Excepteur sint occaecat cupidatat non proident, sunt in culpa qui officia deserunt mollit anim id est laborum.

SmartThings Resources

< Previous Step Next Step >

2. Choose Your Hardware Platform

The first choice you’re likely to face is which protocol to use, Wi-Fi or Thread. If your Matter application requires efficient mesh networking with energy-efficient and robust wireless connectivity, then Thread is the optimal choice. If you need low-power functionality and want to maximize connectivity in the marketplace, Wi-Fi is the well-known universal standard for wireless connectivity in Matter.

We need to guide customers on when a bridge makes the most sense to provide compatibility with existing systems.

We should also provide guidance on what to do if the device type is not covered by Matter today. 

Matter over Thread

The MG24 SoC is a single-chip solution for Matter over Thread, delivering exceptional RF performance, advanced security features with Silicon Labs' Secure Vault™, and low power.

Choose a Thread certified SoC, module, or radio board for end nodes. Matter uses Bluetooth Low Energy for commissioning, so ensure your hardware of choice also supports Bluetooth.  See below to choose the optimal hardware for you.

In the next step get a hardware board for the host of the Thread border router — such as Raspberry Pi or BeagleBoard to run the Matter border router to establish the Thread network. Select a radio co-processor (RCP) compatible development kit — the RCP takes care of the wireless communications operated by the border router.

Select the appropriate development kit for your Matter over Thread end device. 

 

EFR32MG24 Series 2 Modules

EFR32MG24 SoCs

EFR32MG21 Modules

EFR32MG21 SOCs

Flash/RAM   1536/256 kB 1536/256 kB 1024/96 kB 1024/96 kB
Max TX Power  +19.9 dBm +20 dBm +20 dBm +20 dBm
Package Type   PCB/SiP QFN40/QFN48 PCB/SiP QFN32
BLE   Yes Yes Yes Yes
FSK - Sub-GHz   No No Yes Yes
CSS          
Secure Vault   High, Mid High, Mid    
For Battery Power          
  Learn More Learn More Learn More Learn More

Matter over Wi-Fi

The RS9116 NCP or the WF200, coupled with the MG24 as a host, enables Matter over Wi-Fi, with the RS9116 NCP offering the lowest Wi-Fi power consumption in the industry.

Choose a RS9116 NCP or WF200 Wi-Fi co-processor or a certified module to develop Matter over Wi-Fi end devices. See below to choose the optimal hardware for you.

Get the EFR32MG24 host processor to connect to the Wi-Fi NCP and RCP over the SPI host interface.

In the next step, select the appropriate development kit for your Matter over Wi-Fi end device.

 

RS9116 Wi-Fi NCP SoCs

RS9116 Wi-Fi NCP Modules

WF200 Series 2 Wi-Fi Transceiver Modules

WF200 Series 2 Wi-Fi Transceiver SOCs

Flash   4096 kB 4096 kB    
Onboard IP Support Yes      
Key Peripherals  UART, SPI, SDIO, USB, CDC UART, SPI, SDIO, USB, CDC SDIO/SPI SDIO/SPI
  Learn More Learn More Learn More Learn More
< Previous Step Next Step >

Matter Development Kits

Silicon Labs offers several Matter compliant development kits for Thread and Wi-Fi ranging from compact, feature-packed low-cost prototyping platforms to multi-node advanced multiprotocol kits for robust, secure mesh networks. Based on your hardware platform selection in the previous step, select which kit is the best fit for your needs below.

Series 2 Development Kits for Matter over Thread End Devices and Border Routers

The EFR32xG24 Development Kits provide a variety of different hardware options, optimized for your development needs.  Whether it is rapid prototyping using the Explorer Kits, proof of concept and advanced feature development using the Dev Kits, or full development including advanced RF and power consumption testing using the Pro Kits, Silicon Labs has the right development hardware to meet your needs for Matter over Thread development.


 Series 2 Development Kits for OpenThread Border Routers

The EFR32xG21 Development Kits enable enhanced RF development using the Pro Kits that enable advanced RF development and debug capabilities. Including packet trace, to ensure robust RF solutions for Open Thread Border Routers.

Development Kits for Wi-Fi over Matter

Full-featured application development kits.

WF200 Wi-Fi Expansion Kit with Raspberry Pi

The SLEXP8022C WF200 Wi-Fi Expansion kit + Raspberry Pi includes a built-in Raspberry Pi Connector to get started immediately with Linux development and an EXP Connector to enable development on Silicon Labs' MCUs and Wireless MCUs.

MSRP $230.23

WFM200S Wi-Fi Expansion Kit with Raspberry Pi

The SLEXP8023C WFM200S Wi-Fi Expansion kit + Raspberry Pi includes a built-in Raspberry Pi Connector to get started immediately with Linux development and an EXP Connector to enable development on Silicon Labs' MCUs and Wireless MCUs.

MSRP $99.00

< Previous Step Next Step >

4. Create User Accounts

While you wait for your Pro Kit, we recommend setting up your user accounts. If you already have the accounts listed below, you can skip this step. If not, here’s what you’ll need:

Silicon Labs Account:

Silicon Labs Account: This account will offer you access to our developer community, Getting Started guides, private GitHub repositories and our Simplicity Studio development environment. You can create your account or verify access to your account here.

Silicon Labs - Amazon Sidewalk

Join the Connectivity Standards Alliance

To use the Matter specification and certify your Matter product, you will need to be a member of the CSA. You will need to get your own unique Vendor ID (VID) and Product ID (PID).Visit the CSA and decide which membership level is best for you.

Create your Alexa and AWS Accounts.

Silicon Labs - Amazon Sidewalk

Create Amazon Alexa Account:

Amazon Alexa Account: Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat.

Create AWS Account:

Amazon Web Services Account: To connect your device to the cloud, you will need an AWS account. Note: you will need to know if you are a root user or an IAM user. If you’re a new developer, then we recommend setting up a root user account. If you’re an experienced developer, then an IAM user account is right for you. You will be prompted to add your payment and billing details to secure cloud connection. AWS offers a multitude of configuration tools to support you along your journey. More to come on that in the following steps.

Amazon Web Services Logo

Create your Google Home Accounts.

Silicon Labs - Amazon Sidewalk

Google Account:

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat.

Matter Project:

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat.

Silicon Labs - Amazon Sidewalk
Silicon Labs - Amazon Sidewalk

Partner Marketing Hub:

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat.

Create your Samsung SmartThings Accounts.

Silicon Labs - Amazon Sidewalk

SmartThings Developer Account:

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation ullamco laboris nisi ut aliquip ex ea commodo consequat.

< Previous Step Next Step >

5. Set Up Development Environment

We know you have many options when it comes to choosing your development environment, but we believe Simplicity Studio is the right choice for developing your device with Matter. Here’s why:

  • Includes your programmer and debugger functions so you don’t have to worry about manual setup.
  • Automatically recognizes the boards you’ve purchased and filters out sample apps that are not applicable; only exposes the sample apps that are related to your hardware selection.
  • Potentially saving you hours of time in installation, setup and configuration.
  • Simplicity Studio links directly to the private GitHub repositories.
  • Need help setting up your environment? Our Getting Started Guide will have you up and running in no time. 

Download the Full Online Installer Version of Simplicity Studio v5:

System Requirements

Windows     Windows 10 (64-bit)
Windows 11
MacOS 10.14 Mojave
10.15 Catalina*
11.x Big Sur*
12.x Monterey*
*if trying to use the Keil 8051 or IAR toolchains, click here
Linux Ubuntu 20.24 LTS

 

CPU     1 GHz or better
Memory 1 GB RAM (8 GB rcommended for wireless protocol development
Disk Space 600 MB disk space for minimum FFD installation
7 GB for wireless dynamic protocol support
< Previous Step Next Step >
< Previous Step Next Step >

Test & Iterate

In this step, it is important to test your product before submitting to test labs to ensure your product will pass. Testing your product against a Matter Test Harness helps ensure compliance with the spec.

In addition, testing your products with the various Ecosystems provides additional assurance and is required if you want to use their “works with” badges.

< Previous Step Next Step >

Certify Product

These resources will be help you navigate Matter certification.

Tech Talk

Certifying a Matter Device: Thread & Wi-Fi

Learn how to certify your Matter device, focusing on Matter certification for Thread and Wi-Fi devices from our expert engineers in our on-demand training.

< Previous Step Next Step >

Manufacture Product

Silicon Labs Secure Vault + Custom Part Manufacturing Service (CPMS) enables Matter Security.

EFR32MG24 Series 2 Modules
EFR32MG24 SoCs
EFR32MG21 Modules
EFR32MG21 SOCs
RS9116 Wi-Fi NCP SoCs
RS9116 Wi-Fi NCP Modules
WF200 Series 2 Wi-Fi Transceiver Modules
WF200 Series 2 Wi-Fi Transceiver SOCs

If you need help with your purchase, please fill out the form to get connected with a member of our team who can support you.

< Previous Step Next Step >

Operate Product

Monitor operating of products in field.

Provide over the air updates for bug fixes and feature enhancements.

< Previous Step Next Step >
Getting Started
1. Learn and Explore
2. Choose Your Hardware Platform
3. Buy Your Dev Kit
4. Create User Accounts
5. Set Up Dev Environment
Develop
1. Develop Your Product
2. Test & Iterate
3. Certify Product
Deploy Product
1. Manufacture Product
2. Operate Product
Close
Loading Results
Close
STAGING-PUB1