Video Material

BLE-117: Bluetooth LE Power Control

Bluetooth Applications
This material is 1 of 3 in the Bluetooth 104 - Applications: 5.1 and 5.2 Series.

This Bluetooth applications training introduces new enhancements from Bluetooth 5.1 and 5.2 and how Bluetooth designs can benefit from these updates.

Overview

LE Power Control is a new feature introduced in Bluetooth 5.2. The ability to change the TX Power of a device can optimize power efficiency. Before 5.2 there was no standard solution to feedback the signal strength to the transmitter. However, LE Power solves this problem.

Close
Loading Results
Close
STAGING-PUB1