SLWSTK-COEXBP
MSRP $149.00
MSRP $149.00
OVERVIEW
- Enables prototyping of a managed coexistence solution
- Supports Silicon Labs Zigbee, Thread and Bluetooth devices
- Supports Wi-Fi and up to 3 additional WSKT radio boards
- Supports 1, 2 and 3 wire PTA signaling
- Provides header for observation of PTA signals on logic analyzer
- Supports both SoC and NCP software architectures
GETTING STARTED
Step 1: Get Started with Documentation
Review documentation available in the Tech Docs tab above
- Covers the basic concepts behind Wi-Fi Coexistence, helping developers understand the principles that lead to a more robust wireless link in a heavily congested Wi-Fi environment
- UG103.17: Wi-Fi Coexistence Fundamentals
- Understand how the Silicon Labs Coexistence kit will help developers better their design
- UG350: Silicon Labs Coexistence Development Kit
- Understand the nuances of Wi-Fi Coexistence when used with your selected protocol
- AN1017: Zigbee and Thread Coexistence with Wi-Fi
- AN1128: Bluetooth Coexistence with Wi-Fi
Step 2: Configure the Wi-Fi Coexistence and Perform Testing
- Using a PTA capable Wi-Fi solution, configure the PTA interface on the EFR32 based Bluetooth, Zigbee or Thread solution along with the PTA interface of your Wi-Fi device using the instructions and guidance found in UG103.17, UG350, AN1017 and AN1128.
- Use the SLWSTK-COEXBP kit to test and evaluate the PTA performance of your solution which should include throughput scenarios for your application.
NOTE: Not all Wi-Fi solutions are capable of supporting PTA. When choosing a Wi-Fi solution, be sure to select a vendor and a Wi-F solution that supports coexistence/PTA operation.
TECH DOCS
COMMUNITY & SUPPORT
Knowledge Base Articles
Browse our knowledge base articles for information about specific products.
User Forums
Browse technical questions, share your ideas, and learn more about our latest solutions.
Questions? You're in the Right Place.
Silicon Labs has an active, knowledgeable user community of engineers and developers that are enthusiastic about solving problems.