Written Material

PRP-106: RAIL Tutorial - Calibrations

This material is 7 of 8 in the Proprietary 100 - RAIL Tutorial: Beginner.

Review the ordered list of our RAIL Tutorial which is designed to help you get started developing useful applications with RAIL, from basic to advanced features.

Overview

An overview of implementing temperature and image rejection calibrations to reach the maximum performance of the radio; important concepts such as how, when and why calibrations are performed, the drawbacks of performing calibrations, and what happens if calibrations aren’t done are also discussed in this tutorial.

Close
Loading Results
Close
STAGING-PUB2