Overview
With Silicon Labs' software and hardware, you can design a single product that supports multiple wireless connectivity protocols. During our 3-day online webinar series, we will spend an hour each day developing a Bluetooth and Proprietary multiprotocol project with the Thunderboard Sense 2.
Day 1 we will briefly discuss Silicon Labs’ Bluetooth stack and introduce Simplicity Studio. We will walkthrough developing a Bluetooth project using the GATT editor in Simplicity Studio. By the end of the lab, we will use our Blue Gecko mobile phone app to modify the Thunderboard Sense’s RGB LEDs using the device’s GATT characteristics.
Note: At least two Thunderboard Sense 2s are recommended to test a network on Days 2 and 3. However you can still walk through the labs using a single board.