Video Material

BLE-144: Code - Quickly Add an Accelerometer with SPI

This material is 4 of 4 in the Bluetooth 185 - Workshop (SSv5): Quickly Add an Acclerometer With SPI.

This Bluetooth workshop provides hands-on training and teaches users how to quickly add an accelerometer to your IoT device. The project uses Simplicity Studio v5 and the Thunderboard BG22. This training shows how to enable a client to subscribe to BLE notifications transmitting the IMU sensor data.

Overview

This is the final part of the training to introduce how to quickly add an accelerometer with SPI. This video provides an explanation for the code that is required to configure the TDK Invensense IMU sensor in the project.  It explains the code in the provided project files.

Prerequisites:

BG22 Workshop Pre-work

BG22 Getting Started Workshop (Complete Lab 1)

Lab Procedure:

Quickly Add and Accelerometer with SPI

Hardware Required:

Thunderboard Kit EFR32BG22
(SLTB010A)

Close
Loading Results
Close
STAGING-PUB2