Video Material

BLE-154: How to Add a Standard Bluetooth Service to Your Project (Part 3 - Demo)

This material is 3 of 4 in the Bluetooth 188 - Workshop (SSv5): How to Add a Standard Bluetooth Service to Your Project.

This Bluetooth workshop provides hands-on training and teaches users how to add a standard Bluetooth service to an IoT project. The project uses Simplicity Studio v5 and the Thunderboard BG22. This training shows how a Standard Bluetooth service communicates data in a known format to mobile apps so any device can decode the information.

Overview

This video covers the 3rd part of the BG22 workshop focused on adding a Standard Bluetooth Service to a project.  The project programmed in the BG22 Thunderboard is tested using the EFR Connect mobile application.  Viewers learn how the EFR Connect app can be used to view the Bluetooth SIG standard service, identified as Humidity and Temperature.  The project added the Environmental Sensing service and the EFR Connect mobile app displays the values read from the board.

Close
Loading Results
Close
STAGING-PUB2